AXIS#.SAFE.TEMPWARNING.ACTIVE

Description

Indicates whether the SMM temperature is in the expected range.

Value Description

0

SMM temperature is not in the expected range

1

SMM temperature is ok

Versions

Action

Version

Notes

Implemented

2-00-00-000

Implemented in SMM revision v0.56

General Information

Type

Read Only

Units

N/A

Range

0, 1
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
AXIS1.SAFE.TEMPWARNING.ACTIVE

2062h

00h

Unsigned8

-

-

Read only

Yes

AXIS2.SAFE.TEMPWARNING.ACTIVE

2162h

00h

Unsigned8

-

-

Read only

Yes